Now it’s even easier to configure Front Panels and generate 3D drawings
The state-of-the-art nVent SCHROFF Front Panel Configurator tool offers a drag-and-drop function to easily configure and customize front panels. In addition, 3D CAD drawings, bills of materials, quotations and graphics are generated in real time to save design engineers time and hassle. Now, to make it even easier, faster and more accurate for users to design front panels, the configurator offers enhanced visual reference and measurement tools:
- Quick visual reference tools – Newly designed icons provide easier visual reference, and are organized into categories for faster menu selection. Color coatings for the front panel surfaces also are now grouped, so users can quickly view and choose from the array of options. In addition, the updated product view is now capable of embedding textures, transparency, shadows and lights for fuller visual understanding of how the panels will look once installed.
- New measurement tools for faster precision – The new point-to-point (also called edge-to-edge) measurement tool, bounding box dimension and cut-view for each axis make it easier to determine where to add holes, cutouts and other components, such as handles, connectors, LED lights, etc., for the right fit and overall configuration. Plus, if need be, users can fade in the external dimensions of their front panel.
These enhancements are folded into the user-friendly Front Panel configurator.
As part of our commitment to innovation, nVent will continue to make improvements to nVent SCHROFF configurators and suite of online tools and resources to support customers in their engineering work. Stay tuned for future updates!
Get a full overview of the Front Panel Configurator